Technical FAQs

Ask a Question

How can the incoming section be eliminated on a single HVL switch?

Issue:
How can the incoming section be eliminated on a single HVL switch?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
If a single HVL switch is returning an incoming line section, try to reduce the cable size or the numbers of cables per phase.

A larger cable has a larger bend radius. The minimum recommended bend radius of a cable is 12 times the diameter.


CTA-ID : 2011875
Was this helpful?
What can we do to improve the information ?