Technical FAQs

Ask a Question

For 5 & 15kV HVL/cc, what will cause the switch section to increase in width from 14.75`` to 20.00``?

5 & 15kV HVL/cc switch sections will increase in width from 14.75`` to 20.00 if the switch has double barrel fuses or surge arresters above 12kV.


CTA-ID : 2011873
Was this helpful?
What can we do to improve the information ?