Technical FAQs

Ask a Question

Can Fuselogic trip both switches in a duplex arrangement? HVL and HVL/cc?

NO. Fuselogic cannot be used used to trip both switches in a duplex configuration. Neither HVL and HVL/cc. The fuse activates a mechanical rod on the switch, which in turn trips the switch by releasing the trip latch. This rod is required on each switch with a set of fuses. Dual Main is the arrangement that works.

CTA-ID : 2011872
Was this helpful?
What can we do to improve the information ?