Technical FAQs

Ask a Question

Are e-coil conversation kits available to convert 8502SG or 8536SG NEMA size 5 from Series A to Series B ?

Conversions kits are available for control voltages up to 480 volts and can be obtained by ordering one of the following conversion kits.


120 volt = 9998SG120
208 volt = 9998SG208
240 volt = 9998SG240
277 volt = 9998SG277
480 volt = 9998SG480


CTA-ID : 2011741
Was this helpful?
What can we do to improve the information ?