Technical FAQs

Ask a Question

What are the dimensions and weight on the ATS46C41N?

Entire Width a = 15.8 in (401 mm),  Entire Heigth b = 37.4in (950mm), Entire Depth c = 13.9 in (353 mm) and the weight is 123 lbs (56 kg)


CTA-ID : 2011275
Was this helpful?
What can we do to improve the information ?