Technical FAQs

Ask a Question

What are the dimensions and the weight on the ATV28 Frame size 5 drive?

Issue:   What are the dimensions and the weight on the ATV28 Frame size 5 drive?
 
Product Line:   ATV28
 
Environment:  ATV28D16N4 ATv28D23N4
 
Cause:   N/A
 
Resolution:   The entire width of the unit is a = 9.8 in (245 mm), the entire height of unit is b = 13.2 in (330 mm), the entire depth of the unit is c = 7.8 in (195 mm), and the weight is 126 lb (57 kg).

This is the same for the ... D16N4 , D23N4 which are both frame size 5.


 
Was this helpful?
What can we do to improve the information ?