Technical FAQs

Ask a Question

Can we do Main Main Closed Transition automatic transfers.

Yes. We do both open and closed transitons.

With the closed transition, the customer must be sure that there is no problem when the two sources are paralleled. (Such as synchronization)

Both switches will be closed for a predetermined period of time.



CTA-ID : 2011544
Was this helpful?
What can we do to improve the information ?