Technical FAQs

Ask a Question

Where can I get dimensions and data on the obsolete 58M Drive?

Obtain a copy of 30072-450-71 Instruction Bullentin.
``Class 8839 58M Adjustable Speed Drive Controllers, 1 to 75 hp CT and 1 to 100 hp VT, 460 Vac and 1 to 40 hp CT and 1 to 50 hp VT, 208/230 Vac``


CTA-ID : 2010950
Was this helpful?
What can we do to improve the information ?