Technical FAQs

Ask a Question

What is the timing range of a pneumatic relay 9050BO1E?

Timing range: 0.05 second to 3 minutes for timers without micrometer dial. For timers with micrometer dial the timing range is 0.2 seconds to 3 minutes. Note: most type B and C timing relays witthout micrometer dial can be adjusted to 20 minutes. Due to manufacturing tolerances nut every timer can be guaranteed adjustable from 3 to 20 minutes.
Repeat Accuracy:
+/- 10% to 3 minutes
+/- 12% to 5 minutes
+/- 40% to 20 minutes

CTA-ID : 2011352
Was this helpful?
What can we do to improve the information ?