Technical FAQs

Ask a Question

What input types are available for the Analog input AI1 on the ATV11?

It can be voltage: 0-5 V or 0-10 V, impedance 40 K Ohms.
For current: 0-20 mA or 4-20 mA (without added resistance), impedance 250 Ohms.
The input can not be set up for 20-0 or 20-4 mA.

CTA-ID : 2010458
Was this helpful?
What can we do to improve the information ?