Technical FAQs

Ask a Question

Is it OK to convert a fused HVL/cc to unfused with dummy fuse links?<br />Question was from Ken Beard in Canada also.

Yes is OK to convert from fused HVL/cc to Unfused.
Be sure that the available fault current is 25kA Symmetrical or below. This is the unfused rating of the switch.
The fuse panel is interlocked with the switch so that the dummy fuse links not accessible with the switch closed.

CTA-ID : 2011539
Was this helpful?
What can we do to improve the information ?