Technical FAQs

Ask a Question

Will the QOT tandem branch breakers fit in any space in a QO load center?

Issue:
Product Features

Product Line:
QO Load centers

Environment:
Tandem branch breakers

Cause:
Application

Resolution:
No, the QOT tandem branch breakers, will ONLY mount in the positions of a QO load center that have a pan rail slot to accept the mounting CAM ( or hook).



CTA-ID : 2012067
Was this helpful?
What can we do to improve the information ?