Technical FAQs

Ask a Question

Can the HVL switch have the operating handle moved from the left to the right side of the switch? Can the handle be moved to the side of the switch?<br /><br />These are for OEM - Kinney Electric.

No the HVL switch cannot have the operating handle moved from the left to the right side of the switch.

No, the handle cannot be moved to the right side of the switch.


CTA-ID : 2011866
Was this helpful?
What can we do to improve the information ?