Technical FAQs

Ask a Question

How much should the ATV58 be derated for high elevations?

3300 ft (1000 m) maximum without derating; derate the output current by 1% for each additional 330 ft (100 m)


CTA-ID : 2011733
Was this helpful?
What can we do to improve the information ?