Technical FAQs

Ask a Question

What contact blocks should be used with the 9001K85 alternate action module?

The standard normally closed contacts can be used, but for a normally open contact the normally open early closing version must be used. Either a 9001KA4 or a 9001KA6 contact block should be used for normally open contact.

CTA-ID : 2011728
Was this helpful?
What can we do to improve the information ?