Technical FAQs

Ask a Question

One of Bill`s consultant is asking if he could mount one end of metal-clad swgr against the wall.

The reply was that Yes, metal-clad swgr can be mounted against the wall with the consideration of front doors swing to the opposite side.

CTA-ID : 2011721
Was this helpful?
What can we do to improve the information ?