Technical FAQs

Ask a Question

Can you discuss remote tripping on HVL/cc per Drawing C16666924-001-01?

Additional trip contacts can be wired in parallel with the other contacts. Remote trip is wired out to terminal blocks when required.


CTA-ID : 2011536
Was this helpful?
What can we do to improve the information ?