Technical FAQs

Ask a Question

Does the DSFLN unit come with a face plate? I want to use a DFPFN faceplate on 20 of those units.

The DSFLN includes a faceplate with a 1.4`` diameter opening. The DFPFN is an interchangeable face plate that is ordered separately and can be used in place of the standard DSFLN faceplate.

CTA-ID : 2011533
Was this helpful?
What can we do to improve the information ?