Technical FAQs

Ask a Question

Where are the ventilation louvers on HVL?<br /><br />

On indoor units there are no ventilation louvers required.

On outdoor units the the ventilation louvers are in the rear panels or rear doors.


CTA-ID : 2011531
Was this helpful?
What can we do to improve the information ?