Technical FAQs

Ask a Question

Where are the ventilation louvers on HVL/cc?<br /><br />

On indoor units there are no ventilation louvers required.

On outdoor units the ventilation louvers are in the front and back of the roof overhang.


CTA-ID : 2011528
Was this helpful?
What can we do to improve the information ?