Technical FAQs

Ask a Question

Why should the Modbus/Unitelway option card VW3A58303U be used on the ATV58 since the drive can communicate from the keypad port?

The purpose of the card is to allow the keypad port to be available for use of the keypad.
Many customers want to communicate via Modbus but still want to have the keypad for display.

CTA-ID : 2011529
Was this helpful?
What can we do to improve the information ?