Technical FAQs

Ask a Question

MiniBreak Questions:<br />1. What is the spacing between the back plate and the rear of the enclosure if the top exit is available?<br />2. What is the weight for 1-HVMB305000U? <br />3. Is it possible to have the incoming and outgoing by top?<br />4. Do we have copper ground bus, size of 6mmX50mm with two lugs of 4/0 awg?<br />5. What is the color paint? ANSI 49 or ANSI 61?<br />6. Do we have Have we the crimp lugs option? If yes, lugs will be 3 x no 2/0 copper #XLPE100% is it Ok? If not, I believe we can make field installationi is it? <br /><br />

1. 6.75``
2. 450#
3. Yes
4. Ground Bar Only with box lugs for nine #14 - 1/0 Cables
5. ANSI 61
6. NO, 2 lugs maximum No Crimp Lug Option - Set Screw #14-2/0. Lug pad is 1-3/4`` Square 1/8`` thick with hole for 1/4`` bolt.

CTA-ID : 2011526
Was this helpful?
What can we do to improve the information ?