Technical FAQs

Ask a Question

What is the voltage range on the ATV58?

Voltage ratings are as follows:
208 V -15% to 230 V +15% single-phase input
208 V -15% to 230 V +15% three-phase input
400 V -15% to 460 V + 20% three-phase input [See Note 1]

**NOTE 1**  Input voltage is 460 V, -10%, +15% on ATV58HU54N4X-D23N4X controllers as rated in Table 10 on page 16 of VVDED39704US R8/01. Input voltage is 400 V -15% to 460 V +10% on ATV58HC13N4X-C33N4X.
NOTE: The 460 VAC rated drives can also be used in 380 VAC, 50 Hz applications. This includes the ATV58HU54N4X to D23N4X controllers when used without an EMC filter.


CTA-ID : 2011907
Was this helpful?
What can we do to improve the information ?