Technical FAQs

Ask a Question

Is it possible to do in one section with 3-500kcmil cables per phase in the top and 3-500kcmil out the top? 18 cables total.

Yes, it is possible to do in one section with 3-500kcmil cables per phase in the top and 3-500kcmil out the top? 18 cables total.

Need a 36`` Pullbox on top
Need a load side connector assembly
Need both sides with cutouts and cover plates.

This will have to be tagged into the Product Selector.

The Product Selector does not support FRONT ACCESS ONLY for HVL switchgear.


CTA-ID : 2011862
Was this helpful?
What can we do to improve the information ?