Technical FAQs

Ask a Question

Why can`t I pick a 4160V 3 wire ungrounded delta system in the Medium Voltage Metal Enclosed Product Selector.<br /><br />

4160V 3 wire ungrounded delta system is not loaded in the Medium Voltage Metal Enclosed Product Selector. HVL/cc
This is an uncommon system voltage and only the most standard voltages are loaded into the product selector.

The voltages which are allowed for 3 wire delta ungrounded are:
2400, 4800, 4800 (future 13200), 6900, 10000, 11000, 13800, 14400, 16500, 20780, 22860, 23000, 24940.



CTA-ID : 2011860
Was this helpful?
What can we do to improve the information ?