Technical FAQs

Ask a Question

Is top entry acceptable for the MiniBreak switch?<br />Needs a drawing showing conduit area at the top of the switch.

Yes, top entry acceptable for the MiniBreak switch. Although the best entry is bottom. The enclosure is N3R standard and is very well sealed for bottom entry.
There is not a drawing showing conduit area at the top of the switch because bottom is recommended, but the top area would be the same as the bottom.
MiniBreak drawings are on the intranet and internet. How to find below:

DIGEST DRAWINGS - INTRANET

SALES AND MARKETING
INTEGRATED MKTG COMMUNICATION
CAD DRAWINGS
6000 SWITCHGEAR
6040 HVL DIGEST DRAWINGS
6042 MINIBREAK DIGEST DRAWINGS

DIGEST DRAWINGS - INTERNET

SQUARED.COM
SALES AND MARKETING
INTEGRATED MARKETING COMMUNICATION
CAD DRAWINGS
6000 SWITCHGEAR
6040 HVL AND 6042 MINIBREAK DRAWINGS




CTA-ID : 2011859
Was this helpful?
What can we do to improve the information ?