Technical FAQs

Ask a Question

What is the surest way to signal the Altivar ATV66 drive to stop regardless of the mode of operation it is in?

Break LI1 to +24 volts, this takes away the run permissive and the drives goes into a freewheel stop.

This logic input is active whether in serial communications, terminal strip or keypad command and must always be high in order for unit to operate.


CTA-ID : 6918
Was this helpful?
What can we do to improve the information ?