Technical FAQs

Ask a Question

What is the contactor part number and coil voltage that we use for the shorting contactors on the ATS48C11Y starter?

The part number for the shorting contactor is LC1D115.

All the coils for the shorting contactors are selected for 120v, 60hz operation.  The code for this would be to add G7 at end of part # provided.


CTA-ID : 2011714
Was this helpful?
What can we do to improve the information ?