Technical FAQs

Ask a Question

How much energy can an AFD save?

A drive can only save money if the system can be slowed down and meet load requirements.

It can give some savings in demand charges by acting as a soft starter also.

To calculate the projected energy savings can obtain software offered by Square D to input desired information to form a model of what would expect to see.

(This software came with the earlier version of the Harmonics Calculation Software and should be able to obtain copy from FO or Drives PSG)

CTA-ID : 2011092
Was this helpful?
What can we do to improve the information ?