Technical FAQs

Ask a Question

Can the BFR (Base Frequency) parameter on the ATV28 be accessed after initial power up to change its setting?

NOTE: This procedure returns the drive to factory default settings and remove all settings previously made. Make sure that all settings that have been customized for your application are returned. Otherwise, the equipment may not operate as expected.

NOTE: Please refer to the documentation associated with the product for further information, cautions or warnings that may apply to this issue.

The base frequency can be changed by accessing menu drC (drive menu) and setting FCS (return to factory settings) to YES.
The display will show BFR.  Press enter. The factory default setting of 50 will be displayed. Use the arrows to change the value to 60. Press enter to save.
Change other settings as necessary.

CTA-ID : 2006704
Was this helpful?
What can we do to improve the information ?