Technical FAQs

Ask a Question

Can the ATV66 communicate to Devicenet protocol?

Yes you can. Need to contact Panel-Tech for the protocol pcmcia convertor.

Panel Tech`s phone number 1-800-869-2026. The device part number is DN-3000.

The required Square D options that are needed are the Modbus communication PCMSIA Card Communication carrier or either I/O extension module Phoenix DB15 wiring interface.

CTA-ID : 7183
Was this helpful?
What can we do to improve the information ?