Technical FAQs

Ask a Question

Does the HVL/cc switch comply with ANSI C37.20.7-2001 Guide for Testing Medium-Voltage Metal-Enclosed Switchgear for Internal Arcing Faults<br />Revised 03/06/07

No. HVL/cc is not arc resistant and was not tested per ANSI C37.20.7-2001.


CTA-ID : 2011514
Was this helpful?
What can we do to improve the information ?