Technical FAQs

Ask a Question

Does the HVL/cc switch allow 24VDC operation?

Issue:
Does the HVL/cc switch allow 24VDC operation?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Application.

Resolution:
Yes, the HVL/cc switch does allow 24VDC operation?

On motor operated versions the motor, close and trip circuits must be the same voltage. This is true because these circuits are on printed circuit boards.


CTA-ID : 2011857
Was this helpful?
What can we do to improve the information ?