Technical FAQs

Ask a Question

What key lock is used with the HVL Digest Switches?

Issue:
What key lock is used with the HVL Digest Switches?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Key locks used with the HVL Digest Switches:

These are Schneider Canada Key Lock Numbers:

For the switch handle: VFL000010SH
For fuse door: VDL000010SH

Both locks must be odered if key locks are used.


CTA-ID : 2011856
Was this helpful?
What can we do to improve the information ?