Technical FAQs

Ask a Question

What would lock you out of the HVL/cc switch with the SEM mechanism?<br /><br />All the required fields have been filled in. Control Voltages.<br /><br /><br /><br />

Be sure to enter the correct voltages for the product.
HVL and HVL/cc SEM mechansim control voltages:

For the HVL Stored Enengy Mechanism (SEM):
Motor operator voltages are 120VAC or 125VDC.
Trip and close voltages are 48VDC, 120VAC, 125VDC, 240VAC and 250VDC.

For the HVL/cc Stored Enengy Mechanism (SEM):
Motor Operator, Close and Trip voltages are 24VDC, 48VDC, 125VDC, 250VDC, 120VAC and 240VAC.



CTA-ID : 2011851
Was this helpful?
What can we do to improve the information ?