Technical FAQs

Ask a Question

What is the difference between the PAF362000 and the PAF2036?

The PAF362000 includes rating columns for 2000 A, and the PAF2036 is a frame only without rating columns.


CTA-ID : 2011711
Was this helpful?
What can we do to improve the information ?