Technical FAQs

Ask a Question

Is the HOA kit 9999 SC1 replaced by 9999 SC2?

Issue:
Is the HOA kit 9999 SC1 replaced by 9999 SC2?

Product Line:
NEMA Pre-Type S and Type S Accessories

Environment:
Products sold and installed in the US

Cause: 

Replacing obsolete device

Resolution:
No, the 9999 SC1 was a kit for the old style NEMA size 00 devices (8536A series B), which are obsolete.
The 9999 SC2 is too large for use in place of a 9999 SC1.

 
Was this helpful?
What can we do to improve the information ?