Technical FAQs

Ask a Question

On HVL/cc can the surge arresters be connected on the load side of the switch and the line side of the fuse?<br />Surge Arresters are normally connected on the line side of the switch or the load side of the fuse. <br />

YES
This can be done as a special design.
It will require a 29.50`` wide section for 5/15kV HVL/cc only.

The only charge will be for the 29.50`` wide section.


CTA-ID : 2011504
Was this helpful?
What can we do to improve the information ?