Technical FAQs

Ask a Question

Can customer extend beyond the recommended conduit areas shown on the Q2C drawings for HVL.

Yes. Basically the entire bottom is open. Recommended areas are ideal for cables in and out of the same section. If in a lineup with feeders, the feeders only have cables out. This frees up the area that was reserved for the incoming cables. The recommended areas allow for more cable and termination space. They also get the cables out of the way of components which might be mounted in the rear area behind the switch.


CTA-ID : 2011501
Was this helpful?
What can we do to improve the information ?