Technical FAQs

Ask a Question

Are alternate compression lugs available for all the 125amp and 200amp meter socket, Meter-Pak devices?

Issue:
Product Design Features

Product Line:
MP Meter Pak

Environment:
alternate lugs

Cause:
Application

Resolution:
To use Compression lugs on the Meter-Pak devices, need to order the Lug Landing Kit MMSK2 and compression lugs separately.
Also, to meet EUSERC standards, order and install alternate lug landing pad kit MMSK2, and order compression lugs separately.

NOTE: The MMSK2 lug pads are supplied with (2) 1/2"-13 Studs per pad on 1-3/4" centers and keps nuts per NEMA standards.



 
Was this helpful?
What can we do to improve the information ?