Technical FAQs

Ask a Question

What are the approximate dimensions for a ATS46C17N, ATS46C21N, ATS46C25N or ATS46C32N?

The approximate dimensions are 14.34`` (364 mm) W x 26.99`` (685 mm) H x 10.6`` (269 mm) D.
The weight is 97.02 lbs or 44.00 kg.



CTA-ID : 2012023
Was this helpful?
What can we do to improve the information ?