Technical FAQs

Ask a Question

Why does the product selector for 38KV HVL/cc force you to select 2 switches & 2 sets of fuses for a duplex arrangement. The HVL/cc pricing guide appears to have a duplex option with one set of fuses.

The 38KV HVL/cc duplex arranagement with one set of fuses has not been developed yet. We will have to provide 2 switches & 2 sets of fuses for now as provided on the selector. I do not have a timeframe of when this option will be available. However, a note or warning should be added to the selector for future projects.


CTA-ID : 2011846
Was this helpful?
What can we do to improve the information ?