Technical FAQs

Ask a Question

Will the XCSA interlock switch work with 24 volts DC?

Yes. The XCSA713, XCSB713 and XCSC713 all have the 24-48 VAC/DC LED if needed.


CTA-ID : 2011693
Was this helpful?
What can we do to improve the information ?