Technical FAQs

Ask a Question

How is the HVL switch handle linked to the main and flipper blades?

Issue:
How is the HVL switch handle linked to the main and flipper blades?

Product Line:
Medium voltage switchgear.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The HVL switch has direct drive linkage to the blades. No chains are used as with other switch designs. The operating handle is attached to a cam directly attached to the operating shaft. The operating shaft has glastic links attached to the main blades.
There are no chains which might break and prevent the switch blades from opening.


CTA-ID : 2011497
Was this helpful?
What can we do to improve the information ?