Technical FAQs

Ask a Question

Is the QBL22125 breaker and asks if the breaker available in a molded case switch?

Customer was advised that the two pole QBL22000S22 is the molded case switch version of the QBL. This mold case switch will trip under fault currents with a magnitude of 4500a or greater. It has a AIC rating of 10K. The three pole version is QBL32000S22.

CTA-ID : 2011488
Was this helpful?
What can we do to improve the information ?