Technical FAQs

Ask a Question

What are the available control voltages for each product in the Medium Voltage Metal Enclosed Product Selector?<br />

The available control voltages for each product are:

HVL 5/15kV-with OTM Mechanism - Motor 120VAC and 125VDC.
HVL 25/38kV-with OTM Mechanism - Motor 120VAC
HVL 5-38kV- with SEM Mechanism - Motor 120VAC ONLY.
Close and Trip Coil voltages - 48VDC, 120VAC / 125VDC, and 240VAC / 250VDC.

HVL/cc - with OTM or SEM - Motor, Close and Trip voltages - 24VDC, 48VDC, 120VAC / 125VDC, and 240VAC / 250VDC.
NOTE: Motor Operated HVL/cc switches must have Motor, Close and Trip circuits all at the same voltage due to printed circuit board control.
Visi/Vac - Motor, Close and Trip voltages - 48VDC, 120VAC / 125VDC, and 240VAC / 250VDC.





CTA-ID : 2011840
Was this helpful?
What can we do to improve the information ?