Technical FAQs

Ask a Question

Need information on the open/trip question in the product selector.<br />

The open or trip circuit control voltage field will be automatically populated based on the selection of the motor/close voltage. If DC control power is to be provided it should be specified if by the customer or a battery system on a separate line item. In order to be able to select the SEM Shunt Trip Mechanism a trip circuit voltage must be specified.




CTA-ID : 2011839
Was this helpful?
What can we do to improve the information ?