Technical FAQs

Ask a Question

When is it required to answer Charging motor / Close voltage?

Answer charging motor/close voltage if motor operated switches are required, then the operating voltage to be supplied to the motor must be known. For the ``Over Toggle Mechanisms`` (OTM), the motor is used to open and close the switch. If the ``Stored Energy Mechanisms`` (SEM) are required, then the voltage must be specified for the close circuit. Usually the motor and close circuits are the same voltage. They must be on HVL/cc because the circuits are on a standard printed circuit board. FUSELOGIC ``FuseTripping`` requires the SEM Shunt Trip Mechanism and the close voltage must be specified.




CTA-ID : 2011838
Was this helpful?
What can we do to improve the information ?