Technical FAQs

Ask a Question

What is the UL file number for the K and SK and KX operators for use in hazardous locations?

UL file number E10054 (N).
The K SK & KX operators and componets are UL listed for use in hazardous location except as noted in the push button and operator interface catalog 9001CT0001 page 150. The file number is E10054, CCN NOIV.

CTA-ID : 2006391
Was this helpful?
What can we do to improve the information ?