Technical FAQs

Ask a Question

What is the part number for the 4.5`` Enclosure Fan for the 8839 enclosed ATV66 from 1 to 40 HP CT & VTLN and 1 to 50 HP VT 460 VAC drives and 1 to 20 HP CT, VTLN and VT 208/230 VAC drives?

2601631531 is the part number for the 4 and 1/2 inch stirring fan used in the enclosed ATV66 drives. It is operated by 120 VAC from the control transformer in the enclosure. This fan is not actually part of the ATV66 drive and should not be confused with the heatsink, capacitor bank and/or stirring fans that are on some of the ATV66 drives.

CTA-ID : 2011393
Was this helpful?
What can we do to improve the information ?